LaminateDrapingDataBuilderSecondaryVectorType Enumeration

NXOpen.CAE.LaminateDrapingDataBuilder.SecondaryVectorType is an alias for NXOpen.CAE.LaminateDrapingDataBuilderSecondaryVectorType

class NXOpen.CAE.LaminateDrapingDataBuilderSecondaryVectorType

Bases: object

Second Alignment Types

Enum Members

Enum Member Enum Member Description
Default
default
Specify
specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.