ModelUpdateDesignVariable Class¶
-
class
NXOpen.CAE.
ModelUpdateDesignVariable
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.CAE.ModelUpdateDesignVariable
, which is a meta-solution used to update finite element models to match real life test dataNew in version NX8.0.1.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetActivityStatus | Gets activity status @return |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDesignVariableModelingObject | Gets the design variable modeling object @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLowerBound | Gets lower bound @return |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUpperBound | Gets upper bound @return |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetValue | Gets value @return |
GetWeight | Gets weight @return |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetActivityStatus | Sets activity status |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetLowerBound | Sets lower bound |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUpperBound | Sets upper bound |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetValue | Sets value |
SetWeight | Sets weight |
Property Detail¶
IsOccurrence¶
-
ModelUpdateDesignVariable.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ModelUpdateDesignVariable.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ModelUpdateDesignVariable.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ModelUpdateDesignVariable.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ModelUpdateDesignVariable.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ModelUpdateDesignVariable.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
ModelUpdateDesignVariable.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetActivityStatus¶
-
ModelUpdateDesignVariable.
GetActivityStatus
¶ Gets activity status
Signature
GetActivityStatus()
Returns: Return type: bool New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
GetDesignVariableModelingObject¶
-
ModelUpdateDesignVariable.
GetDesignVariableModelingObject
¶ Gets the design variable modeling object
Signature
GetDesignVariableModelingObject()
Returns: Return type: NXOpen.CAE.ModelingObjectPropertyTable
New in version NX8.0.1.
License requirements: None.
GetLowerBound¶
-
ModelUpdateDesignVariable.
GetLowerBound
¶ Gets lower bound
Signature
GetLowerBound()
Returns: Return type: float New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
GetUpperBound¶
-
ModelUpdateDesignVariable.
GetUpperBound
¶ Gets upper bound
Signature
GetUpperBound()
Returns: Return type: float New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
GetValue¶
-
ModelUpdateDesignVariable.
GetValue
¶ Gets value
Signature
GetValue()
Returns: Return type: float New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
GetWeight¶
-
ModelUpdateDesignVariable.
GetWeight
¶ Gets weight
Signature
GetWeight()
Returns: Return type: float New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
Print¶
-
ModelUpdateDesignVariable.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetActivityStatus¶
-
ModelUpdateDesignVariable.
SetActivityStatus
¶ Sets activity status
Signature
SetActivityStatus(active)
Parameters: active (bool) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
SetLowerBound¶
-
ModelUpdateDesignVariable.
SetLowerBound
¶ Sets lower bound
Signature
SetLowerBound(lowerBound)
Parameters: lowerBound (float) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
SetName¶
-
ModelUpdateDesignVariable.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetUpperBound¶
-
ModelUpdateDesignVariable.
SetUpperBound
¶ Sets upper bound
Signature
SetUpperBound(upperBound)
Parameters: upperBound (float) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)