BoltBuilderSpiderDiameter Enumeration

NXOpen.CAE.BoltBuilder.SpiderDiameter is an alias for NXOpen.CAE.BoltBuilderSpiderDiameter

class NXOpen.CAE.BoltBuilderSpiderDiameter

Bases: object

Represents the options for spider diameter

Enum Members

Enum Member Enum Member Description
Relative
Specifies spider diameter relative to hole diameter
Absolute
Specifies spider diameter in absolute terms
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.