LaminatePlyPlyFailureTheoryType Enumeration¶
NXOpen.CAE.LaminatePly.PlyFailureTheoryType is an alias for NXOpen.CAE.LaminatePlyPlyFailureTheoryType
-
class
NXOpen.CAE.
LaminatePlyPlyFailureTheoryType
¶ Bases:
object
Ply failure theory types
Enum Members
Enum Member Enum Member Description NotSet No failure theory selectedHill Hill failure criteriaHoffman Hoffman failure criteriaTsaiWu Tsai-Wu failure criteriaMaxStrain Maximum Strain failure criteriaMaxStress Maximum Stress failure criteriaMaxTransverseShear Maximum Transverse Shear Stress failure criteriaVonMisesYield Von Mises Yield failure criteriaVonMisesUltimate Von Mises Utlimate failure criteriaProgressiveFailure Progressive Failure failure criteriaUserDefined User defined ply failure theory (thru a user dll)-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-