MappedMeshBuilderMidNodeType Enumeration

NXOpen.CAE.MappedMeshBuilder.MidNodeType is an alias for NXOpen.CAE.MappedMeshBuilderMidNodeType

class NXOpen.CAE.MappedMeshBuilderMidNodeType

Bases: object

Mid-node placement options

Enum Members

Enum Member Enum Member Description
Mixed
Mixed Option
Curved
Curved Option
Straight
Straight Option
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.