LaminateSpreadsheetReportBuilderThreshType Enumeration

NXOpen.CAE.LaminateSpreadsheetReportBuilder.ThreshType is an alias for NXOpen.CAE.LaminateSpreadsheetReportBuilderThreshType

class NXOpen.CAE.LaminateSpreadsheetReportBuilderThreshType

Bases: object

The type of threshold used to filter results.

Enum Members

Enum Member Enum Member Description
AboveTreshold
Filter out results above the specified value
BelowTreshold
Filter out results below the specified value
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.