XyFunctionMaterialType Enumeration

class NXOpen.CAE.XyFunctionMaterialType

Bases: object

Defines material purpose type of a function Enum Members

Enum Member Enum Member Description
General
Function is General Function.
Time
Function is Time History
Temperature
Function is Temperature
StressStrain
Function is Stress/Strain Function
Life
Function is Fatigue Life
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.