LaminateDrapingDataBuilder Class

class NXOpen.CAE.LaminateDrapingDataBuilder

Bases: NXOpen.Builder

Represents a NXOpen.CAE.LaminateDrapingData builder

To create a new instance of this class, use NXOpen.CAE.LaminatePly.CreateDrapingDataBuilder()

New in version NX6.0.0.

Properties

Property Description
CutSelection Returns the selected cut curves.
DirectionCsys Returns or sets the draping direction coordinate system
DirectionOption Returns or sets the draping direction option
DrapingAbsMeshSize Returns the absolute draping mesh size
DrapingMeshRatio Returns or sets the draping mesh ratio
DrapingPath Returns or sets the draping path
FaceSelection Returns the selected faces.
LockingAngle Returns the locking angle
PrimaryVector Returns or sets the primary alignment
SecondaryVector Returns or sets the specify
SecondaryVectorChoice Returns or sets the secondary alignment
SeedSelection Returns the selected seed curves.
Solver Returns or sets the solver
StartPoint Returns or sets the start point
Tag Returns the Tag for this object.
UsingDrapingMeshSize Returns or sets the method used

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CutSelection

LaminateDrapingDataBuilder.CutSelection

Returns the selected cut curves.

Can be geometric edges or element edges.

-------------------------------------

Getter Method

Signature CutSelection()

Returns:
Return type:NXOpen.CAE.LaminateSelectEntitiesBuilder

New in version NX7.5.2.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

DirectionCsys

LaminateDrapingDataBuilder.DirectionCsys

Returns or sets the draping direction coordinate system

-------------------------------------

Getter Method

Signature DirectionCsys()

Returns:
Return type:NXOpen.CoordinateSystem

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DirectionCsys(directionCsys)

Parameters:directionCsys (NXOpen.CoordinateSystem) –

New in version NX10.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

DirectionOption

LaminateDrapingDataBuilder.DirectionOption

Returns or sets the draping direction option

-------------------------------------

Getter Method

Signature DirectionOption()

Returns:
Return type:NXOpen.CAE.LaminateDrapingDataBuilderDrapingDirectionType

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DirectionOption(directionOption)

Parameters:directionOption (NXOpen.CAE.LaminateDrapingDataBuilderDrapingDirectionType) –

New in version NX10.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

DrapingAbsMeshSize

LaminateDrapingDataBuilder.DrapingAbsMeshSize

Returns the absolute draping mesh size

-------------------------------------

Getter Method

Signature DrapingAbsMeshSize()

Returns:
Return type:NXOpen.Expression

New in version NX8.5.1.

License requirements: None.

DrapingMeshRatio

LaminateDrapingDataBuilder.DrapingMeshRatio

Returns or sets the draping mesh ratio

-------------------------------------

Getter Method

Signature DrapingMeshRatio()

Returns:
Return type:float

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature DrapingMeshRatio(ratio)

Parameters:ratio (float) –

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

DrapingPath

LaminateDrapingDataBuilder.DrapingPath

Returns or sets the draping path

-------------------------------------

Getter Method

Signature DrapingPath()

Returns:
Return type:NXOpen.CAE.LaminateDrapingDataBuilderDrapingPathType

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature DrapingPath(type)

Parameters:type (NXOpen.CAE.LaminateDrapingDataBuilderDrapingPathType) –

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

FaceSelection

LaminateDrapingDataBuilder.FaceSelection

Returns the selected faces.

Can be geometric faces or element faces.

-------------------------------------

Getter Method

Signature FaceSelection()

Returns:
Return type:NXOpen.CAE.LaminateSelectEntitiesBuilder

New in version NX7.5.2.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

LockingAngle

LaminateDrapingDataBuilder.LockingAngle

Returns the locking angle

-------------------------------------

Getter Method

Signature LockingAngle()

Returns:
Return type:NXOpen.Expression

New in version NX8.5.1.

License requirements: None.

PrimaryVector

LaminateDrapingDataBuilder.PrimaryVector

Returns or sets the primary alignment

-------------------------------------

Getter Method

Signature PrimaryVector()

Returns:
Return type:NXOpen.Direction

New in version NX6.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature PrimaryVector(primaryAlignment)

Parameters:primaryAlignment (NXOpen.Direction) –

New in version NX6.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

SecondaryVector

LaminateDrapingDataBuilder.SecondaryVector

Returns or sets the specify

-------------------------------------

Getter Method

Signature SecondaryVector()

Returns:
Return type:NXOpen.Direction

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature SecondaryVector(specify)

Parameters:specify (NXOpen.Direction) –

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

SecondaryVectorChoice

LaminateDrapingDataBuilder.SecondaryVectorChoice

Returns or sets the secondary alignment

-------------------------------------

Getter Method

Signature SecondaryVectorChoice()

Returns:
Return type:NXOpen.CAE.LaminateDrapingDataBuilderSecondaryVectorType

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature SecondaryVectorChoice(secondaryAlignment)

Parameters:secondaryAlignment (NXOpen.CAE.LaminateDrapingDataBuilderSecondaryVectorType) –

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

SeedSelection

LaminateDrapingDataBuilder.SeedSelection

Returns the selected seed curves.

Can be geometric edges or element edges.

-------------------------------------

Getter Method

Signature SeedSelection()

Returns:
Return type:NXOpen.CAE.LaminateSelectEntitiesBuilder

New in version NX7.5.2.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

Solver

LaminateDrapingDataBuilder.Solver

Returns or sets the solver

-------------------------------------

Getter Method

Signature Solver()

Returns:
Return type:NXOpen.CAE.LaminateDrapingDataBuilderSolverType

New in version NX6.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature Solver(solver)

Parameters:solver (NXOpen.CAE.LaminateDrapingDataBuilderSolverType) –

New in version NX6.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

StartPoint

LaminateDrapingDataBuilder.StartPoint

Returns or sets the start point

-------------------------------------

Getter Method

Signature StartPoint()

Returns:
Return type:NXOpen.Point

New in version NX6.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature StartPoint(startPoint)

Parameters:startPoint (NXOpen.Point) –

New in version NX6.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

UsingDrapingMeshSize

LaminateDrapingDataBuilder.UsingDrapingMeshSize

Returns or sets the method used

-------------------------------------

Getter Method

Signature UsingDrapingMeshSize()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature UsingDrapingMeshSize(usingSize)

Parameters:usingSize (bool) –

New in version NX7.5.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

Method Detail

Validate

LaminateDrapingDataBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.