BeamEADBuilderOrientationMethod Enumeration

NXOpen.CAE.BeamEADBuilder.OrientationMethod is an alias for NXOpen.CAE.BeamEADBuilderOrientationMethod

class NXOpen.CAE.BeamEADBuilderOrientationMethod

Bases: object

indicates which orientation method to use

Enum Members

Enum Member Enum Member Description
Vector
use a vector to orient the element
Node
use a node to orient the element
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.