FreeBodyResultsBuilderVectorDisplay Enumeration

NXOpen.CAE.FreeBodyResultsBuilder.VectorDisplay is an alias for NXOpen.CAE.FreeBodyResultsBuilderVectorDisplay

class NXOpen.CAE.FreeBodyResultsBuilderVectorDisplay

Bases: object

Vector display option

Enum Members

Enum Member Enum Member Description
Magnitude
display single magnitude vector
Components
display individual components
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.