SimLoadRecipeTypesDataTypes Enumeration¶
NXOpen.CAE.SimLoadRecipeTypes.DataTypes is an alias for NXOpen.CAE.SimLoadRecipeTypesDataTypes
-
class
NXOpen.CAE.
SimLoadRecipeTypesDataTypes
¶ Bases:
object
This enum defines the Data Type options
Enum Members
Enum Member Enum Member Description TimeData Time DataFrequencySpectra Frequency SpectraWaterfallofTimeData Waterfall of Time DataWaterfallofFrequencySpectra Waterfall of Frequency SpectraOrderCut Order Cut-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-