LaminateDynamicSimCollection Class

class NXOpen.CAE.LaminateDynamicSimCollection

Bases: object

Represents a collection of laminate dynamic sims

To obtain an instance of this class, refer to NXOpen.CAE.LaminateManager

New in version NX9.0.0.

Properties

Property Description
Active Returns or sets the active laminate dynamic sim

Methods

Method Description
CloneDynamicSim Clones the laminate dynamic sim
CreateDampingFactorBuilder Creates a builder for the laminate damping factor.
CreateDynamicSimBuilder Creates a builder for the laminate dynamic sim.
Delete Deletes the laminate dynamic sim
FindObject Finds a laminate dynamic sim with the specified name @return Laminate Dynamic Sim found

Property Detail

Active

LaminateDynamicSimCollection.Active

Returns or sets the active laminate dynamic sim

-------------------------------------

Getter Method

Signature Active()

Returns:Active laminate dynamic sim
Return type:NXOpen.CAE.LaminateDynamicSim

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

-------------------------------------

Setter Method

Signature Active(dynamicSim)

Parameters:dynamicSim (NXOpen.CAE.LaminateDynamicSim) – Laminate dynamic sim to be set active

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

Method Detail

CloneDynamicSim

LaminateDynamicSimCollection.CloneDynamicSim

Clones the laminate dynamic sim

Signature CloneDynamicSim(dynamicSim)

Parameters:dynamicSim (NXOpen.CAE.LaminateDynamicSim) – Laminate dynamic sim to be cloned

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

CreateDampingFactorBuilder

LaminateDynamicSimCollection.CreateDampingFactorBuilder

Creates a builder for the laminate damping factor.

Signature CreateDampingFactorBuilder(contextObjectTag)

Parameters:contextObjectTag (NXOpen.TaggedObject) – The metasolution or the mode property.
Returns:
Return type:NXOpen.CAE.LaminateDampingFactorBuilder

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

CreateDynamicSimBuilder

LaminateDynamicSimCollection.CreateDynamicSimBuilder

Creates a builder for the laminate dynamic sim.

Signature CreateDynamicSimBuilder(laminateDynamicSimTag)

Parameters:laminateDynamicSimTag (NXOpen.CAE.LaminateDynamicSim) – The metasolution.
Returns:
Return type:NXOpen.CAE.LaminateDynamicSimBuilder

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

Delete

LaminateDynamicSimCollection.Delete

Deletes the laminate dynamic sim

Signature Delete(dynamicSim)

Parameters:dynamicSim (NXOpen.CAE.LaminateDynamicSim) – Laminate dynamic sim to be deleted

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

FindObject

LaminateDynamicSimCollection.FindObject

Finds a laminate dynamic sim with the specified name

Signature FindObject(name)

Parameters:name (str) – Laminate Dynamic Sim name to be found
Returns:Laminate Dynamic Sim found
Return type:NXOpen.CAE.LaminateDynamicSim

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)