LaminateQuickReportBuilderEnvelopeRule Enumeration

NXOpen.CAE.LaminateQuickReportBuilder.EnvelopeRule is an alias for NXOpen.CAE.LaminateQuickReportBuilderEnvelopeRule

class NXOpen.CAE.LaminateQuickReportBuilderEnvelopeRule

Bases: object

Result enveloping rules.

When there is more than one solutions or loadcases, defines which result to keep and display in the quick report

Enum Members

Enum Member Enum Member Description
MaxMin
Keep minimum and maximum values
Min
Keep minimum values
Max
Keep maximum values
AbsMax
Keep maximum absolute values
AbsMin
Keep minimum absolute values
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.