FunctionCollection Class¶
-
class
NXOpen.CAE.
FunctionCollection
¶ Bases:
object
Represents a collection of function objects
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Copy | Copies a NXOpen.CAE.Function in the Scenario database of Motion Simulation and Advanced Simulation. |
CreateFunctionBuilder | Return NXOpen.CAE.FunctionBuilder object @return |
Delete | Delete a NXOpen.CAE.Function in the Scenario database of Motion Simulation and Advanced Simulation. |
FindObject | Finds the NXOpen.CAE.Function with the given name. |
Method Detail¶
Copy¶
-
FunctionCollection.
Copy
¶ Copies a
NXOpen.CAE.Function
in the Scenario database of Motion Simulation and Advanced Simulation.Signature
Copy(sourceFunction, destinationFunctionName)
Parameters: - sourceFunction (
NXOpen.CAE.Function
) – - destinationFunctionName (str) –
Returns: Return type: New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
- sourceFunction (
CreateFunctionBuilder¶
-
FunctionCollection.
CreateFunctionBuilder
¶ Return
NXOpen.CAE.FunctionBuilder
objectSignature
CreateFunctionBuilder(function)
Parameters: function ( NXOpen.CAE.Function
) –Returns: Return type: NXOpen.CAE.FunctionBuilder
New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Delete¶
-
FunctionCollection.
Delete
¶ Delete a
NXOpen.CAE.Function
in the Scenario database of Motion Simulation and Advanced Simulation.Signature
Delete(deleteFunction)
Parameters: deleteFunction ( NXOpen.CAE.Function
) – the function to be deletedNew in version NX6.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
FindObject¶
-
FunctionCollection.
FindObject
¶ Finds the
NXOpen.CAE.Function
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.CAE.Function
New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)