ModelUpdateOptimOptionsBuilderMethodChoice Enumeration

NXOpen.CAE.ModelUpdateOptimOptionsBuilder.MethodChoice is an alias for NXOpen.CAE.ModelUpdateOptimOptionsBuilderMethodChoice

class NXOpen.CAE.ModelUpdateOptimOptionsBuilderMethodChoice

Bases: object

the method of the optimizer

Enum Members

Enum Member Enum Member Description
LeastSquares
Least Squares method
SteepestDescent
Steepest Descent method
GeneticAlgorithm
Genetic Algorithm method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.