SimSolutionSetupCheckOption Enumeration

NXOpen.CAE.SimSolution.SetupCheckOption is an alias for NXOpen.CAE.SimSolutionSetupCheckOption

class NXOpen.CAE.SimSolutionSetupCheckOption

Bases: object

Model Setup Check Options

Enum Members

Enum Member Enum Member Description
DoNotCheck
do perform any set up checks
CheckAndStopAtFirstError
perform set up checks but stop at first error
CompleteCheckAndOutputErrors
perform all set up checks and report all errors
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.