FEModelOccAttributeRepType Enumeration¶
NXOpen.CAE.FEModelOccAttribute.RepType is an alias for NXOpen.CAE.FEModelOccAttributeRepType
-
class
NXOpen.CAE.
FEModelOccAttributeRepType
¶ Bases:
object
Represents the FemOcc representation type
Enum Members
Enum Member Enum Member Description BaseFem No alternate rep. Use prototype FEM as representationSuperElement Alternate rep is a superelement-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-