ModelUpdateSolutionTargetType Enumeration

NXOpen.CAE.ModelUpdateSolution.TargetType is an alias for NXOpen.CAE.ModelUpdateSolutionTargetType

class NXOpen.CAE.ModelUpdateSolutionTargetType

Bases: object

Represents the type when export to targets and errors to csv file

Enum Members

Enum Member Enum Member Description
All
Export all the targets to the csv file
Frequencies
Export all the frequency targets to the csv file
ModeShapes
Export all the mode shape targets to the csv file
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.