LaminatePostReportBuilder Class¶
-
class
NXOpen.CAE.
LaminatePostReportBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminatePostReport
builderThere is no kf creator.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the name of the laminate post report setup |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSelectedResults | Get the selected results |
GetSelectedSolutions | Get the selected results |
SetSelectedResults | Set the selected results |
SetSelectedSolutions | Set the selected results |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Name¶
-
LaminatePostReportBuilder.
Name
¶ Returns or sets the name of the laminate post report setup
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Method Detail¶
GetSelectedResults¶
-
LaminatePostReportBuilder.
GetSelectedResults
¶ Get the selected results
Signature
GetSelectedResults()
Returns: a tuple Return type: A tuple consisting of (resultNames, loadcaseNames, iterationNames). resultNames is a list of str. loadcaseNames is a list of str. iterationNames is a list of str. New in version NX8.0.0.
Deprecated since version NX11.0.0: Use NXOpen.CAE.LaminatePostReport.GetSelectedSolutions instead.
License requirements: nx_lam_composites (“Laminate Composites”)
GetSelectedSolutions¶
-
LaminatePostReportBuilder.
GetSelectedSolutions
¶ Get the selected results
Signature
GetSelectedSolutions()
Returns: a tuple Return type: A tuple consisting of (solutionNames, selectAllSubcases, loadcaseNames, iterationNames). solutionNames is a list of str. selectAllSubcases is a list of bool. loadcaseNames is a list of str. iterationNames is a list of str. New in version NX11.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
SetSelectedResults¶
-
LaminatePostReportBuilder.
SetSelectedResults
¶ Set the selected results
Signature
SetSelectedResults(resultNames, loadcaseNames, iterationNames)
Parameters: - resultNames (list of str) –
- loadcaseNames (list of str) –
- iterationNames (list of str) –
New in version NX8.0.0.
Deprecated since version NX11.0.0: Use NXOpen.CAE.LaminatePostReport.SetSelectedSolutions instead.
License requirements: nx_lam_composites (“Laminate Composites”)
SetSelectedSolutions¶
-
LaminatePostReportBuilder.
SetSelectedSolutions
¶ Set the selected results
Signature
SetSelectedSolutions(solutionNames, selectAllSubcases, loadcaseNames, iterationNames)
Parameters: - solutionNames (list of str) –
- selectAllSubcases (list of bool) –
- loadcaseNames (list of str) –
- iterationNames (list of str) –
New in version NX11.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Validate¶
-
LaminatePostReportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.