CaeGroupCollectionAutoGroupTypes_Struct Struct¶
NXOpen.CAE.CaeGroupCollection.AutoGroupTypes is an alias for NXOpen.CAE.CaeGroupCollectionAutoGroupTypes_Struct
-
class
NXOpen.CAE.
CaeGroupCollectionAutoGroupTypes_Struct
¶ Bases:
object
Contains information about the types by which we do auto grouping .
Constructor: NXOpen.CAE.CaeGroupCollection.AutoGroupTypes()
Fields¶
Field | Description |
---|---|
ByMaterial | true if meshes are to be grouped by material |
ByPpt | true if meshes are to be grouped by physical property table |
ByColor | true if meshes are to be grouped by color |
BySection | true if meshes are to be grouped by 1-D section |
ByLaminate | true if meshes are to be grouped by laminate |
ByDimension | true if meshes are to be grouped by dimension |
ByMeshcolltype | true if meshes are to be grouped by mesh collector type |
ByMeshsubtype | related to meshes_by_meshcolltype, true if we also want to group by mesh subtype |
ByMaterial¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByMaterial
¶ true if meshes are to be grouped by material
-------------------------------------
Field Value Type:bool
ByPpt¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByPpt
¶ true if meshes are to be grouped by physical property table
-------------------------------------
Field Value Type:bool
ByColor¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByColor
¶ true if meshes are to be grouped by color
-------------------------------------
Field Value Type:bool
BySection¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
BySection
¶ true if meshes are to be grouped by 1-D section
-------------------------------------
Field Value Type:bool
ByLaminate¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByLaminate
¶ true if meshes are to be grouped by laminate
-------------------------------------
Field Value Type:bool
ByDimension¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByDimension
¶ true if meshes are to be grouped by dimension
-------------------------------------
Field Value Type:bool