ManualSweepBetweenSelection Class¶
-
class
NXOpen.CAE.
ManualSweepBetweenSelection
¶ Bases:
NXOpen.Builder
Builder for creating Manual Hex Mesh - Face Dependency type.
To create a new instance of this class, use
NXOpen.CAE.SweepBetweenMeshBuilder.ManualSweepBetween()
New in version NX7.5.2.
Deprecated since version NX10.0.0: Use
CAE.Mesh3dHexBuilder
.
Properties¶
Property | Description |
---|---|
LoopList | Returns the loop list |
MasterFace | Returns the master face |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face |
WallFaceSelection | Returns the Wall face selection |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateNewListItem | The list item @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LoopList¶
-
ManualSweepBetweenSelection.
LoopList
¶ Returns the loop list
-------------------------------------
Getter Method
Signature
LoopList()
Returns: Return type: NXOpen.CAE.ManualSweepBetweenListItemSelectionList
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
MasterFace¶
-
ManualSweepBetweenSelection.
MasterFace
¶ Returns the master face
-------------------------------------
Getter Method
Signature
MasterFace()
Returns: Return type: NXOpen.CAE.SelectCAEFace
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetFace¶
-
ManualSweepBetweenSelection.
TargetFace
¶ Returns the target face
-------------------------------------
Getter Method
Signature
TargetFace()
Returns: Return type: NXOpen.CAE.SelectCAEFace
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
WallFaceSelection¶
-
ManualSweepBetweenSelection.
WallFaceSelection
¶ Returns the Wall face selection
-------------------------------------
Getter Method
Signature
WallFaceSelection()
Returns: Return type: NXOpen.CAE.SelectCAEFaceList
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
CreateNewListItem¶
-
ManualSweepBetweenSelection.
CreateNewListItem
¶ The list item
Signature
CreateNewListItem(tMasterEdge, tTargetEdge, fFlipDirection)
Parameters: - tMasterEdge (
NXOpen.CAE.CAEEdge
) – The master edge - tTargetEdge (
NXOpen.CAE.CAEEdge
) – The target edge - fFlipDirection (bool) – flip direction
Returns: Return type: New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tMasterEdge (
Validate¶
-
ManualSweepBetweenSelection.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.