AfuMathOperationTimeToSrsResponseType Enumeration

NXOpen.CAE.AfuMathOperation.TimeToSrsResponseType is an alias for NXOpen.CAE.AfuMathOperationTimeToSrsResponseType

class NXOpen.CAE.AfuMathOperationTimeToSrsResponseType

Bases: object

Defines the response type paramater for TIME to SRS

Enum Members

Enum Member Enum Member Description
PositiveMax
Positive Maximum
NegativeMax
Negative Maximum
AbsoluteMax
Absolute Maximum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.