PrimitiveMeshBuilder Class¶
-
class
NXOpen.CAE.
PrimitiveMeshBuilder
¶ Bases:
NXOpen.Builder
Represents Primitive Mesh * Used to create a
CAE.Mesh
To create a new instance of this class, use
NXOpen.CAE.MeshManager.CreatePrimitiveMeshBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
ElementType | Returns the element type builder. |
Name | Returns or sets the mesh object name. |
PropertyTable | Returns the property table associated with the mesh. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ElementType¶
-
PrimitiveMeshBuilder.
ElementType
¶ Returns the element type builder.
-------------------------------------
Getter Method
Signature
ElementType()
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Name¶
-
PrimitiveMeshBuilder.
Name
¶ Returns or sets the mesh object name.
-------------------------------------
Getter Method
Signature
Name()
Returns: name of the mesh Return type: str New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – The new name being assigned or set New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
PropertyTable¶
-
PrimitiveMeshBuilder.
PropertyTable
¶ Returns the property table associated with the mesh.
The property table contains the parameters needed for the generation of the mesh.
-------------------------------------
Getter Method
Signature
PropertyTable()
Returns: Mesh property table Return type: NXOpen.CAE.PropertyTable
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
PrimitiveMeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.