MeshControlCollection Class

class NXOpen.CAE.MeshControlCollection

Bases: object

Provides methods for managing mesh controls:py:class:NXOpen.CAE.MeshControl in a fem part

To obtain an instance of this class, refer to NXOpen.CAE.BaseFEModel

New in version NX5.0.0.

Methods

Method Description
CreateBuilder Creates a mesh control builder for the mesh control object @return MeshControl Builder
CreateMmcCreateBuilder Creates a builder for the MMC Create command.
FindObject Finds the NXOpen.CAE.Mesh with the given identifier as recorded in a journal.

Method Detail

CreateBuilder

MeshControlCollection.CreateBuilder

Creates a mesh control builder for the mesh control object

Signature CreateBuilder(meshControl)

Parameters:meshControl (NXOpen.CAE.MeshControl) – NXOpen.CAE.MeshControl to be edited, if None then create a new one
Returns:MeshControl Builder
Return type:NXOpen.CAE.MeshControlBuilder

New in version NX5.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”)

CreateMmcCreateBuilder

MeshControlCollection.CreateMmcCreateBuilder

Creates a builder for the MMC Create command.

Signature CreateMmcCreateBuilder(mmcCreate)

Parameters:mmcCreate (NXOpen.CAE.MeshMate) – NXOpen.CAE.MeshMate to be edited, if None then create a new one
Returns:MMCCreateBuilder
Return type:NXOpen.CAE.MMCCreateBuilder

New in version NX6.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”)

FindObject

MeshControlCollection.FindObject

Finds the NXOpen.CAE.Mesh with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – MeshControl name
Returns:mesh control with this identifier
Return type:NXOpen.CAE.MeshControl

New in version NX3.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”)