FreeBodyResultsBuilderLocationMethod Enumeration

NXOpen.CAE.FreeBodyResultsBuilder.LocationMethod is an alias for NXOpen.CAE.FreeBodyResultsBuilderLocationMethod

class NXOpen.CAE.FreeBodyResultsBuilderLocationMethod

Bases: object

Location definition method

Enum Members

Enum Member Enum Member Description
Id
location is defined by node id
Coords
location is defined by coordinates
Csysorigin
location is defined by coordinate system origin
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.