QueryCurveUsageOptions Class¶
-
class
NXOpen.CAE.
QueryCurveUsageOptions
¶ Bases:
NXOpen.TaggedObject
Represents the options to apply a query curve
This is a sub object
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CurveUsage | Returns or sets the curve usage |
DistanceTolerance | Returns or sets the distance to mesh tolerance |
ProjectDirection | Returns or sets the projection direction |
QueryCurve | Returns or sets the query curve object |
ResultantCurveLocator | Returns or sets the resultant curve locator |
ResultantLocationTolerance | Returns or sets the resultant location tolerance |
ReverseDirection | Returns or sets the reverse direction |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
QueryCurveUsageOptionsCurveUsageType Enumeration | Types of ways query curves can be used |
QueryCurveUsageOptionsResultantCurveLocatorType Enumeration | Where the curve will resolve entities on the curve path |
Property Detail¶
CurveUsage¶
-
QueryCurveUsageOptions.
CurveUsage
¶ Returns or sets the curve usage
-------------------------------------
Getter Method
Signature
CurveUsage()
Returns: Return type: NXOpen.CAE.QueryCurveUsageOptionsCurveUsageType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveUsage(curveUsage)
Parameters: curveUsage ( NXOpen.CAE.QueryCurveUsageOptionsCurveUsageType
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DistanceTolerance¶
-
QueryCurveUsageOptions.
DistanceTolerance
¶ Returns or sets the distance to mesh tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ProjectDirection¶
-
QueryCurveUsageOptions.
ProjectDirection
¶ Returns or sets the projection direction
-------------------------------------
Getter Method
Signature
ProjectDirection()
Returns: Return type: NXOpen.Vector3d
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectDirection(direction)
Parameters: direction ( NXOpen.Vector3d
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
QueryCurve¶
-
QueryCurveUsageOptions.
QueryCurve
¶ Returns or sets the query curve object
-------------------------------------
Getter Method
Signature
QueryCurve()
Returns: Return type: NXOpen.CAE.QueryCurve
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QueryCurve(queryCurve)
Parameters: queryCurve ( NXOpen.CAE.QueryCurve
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ResultantCurveLocator¶
-
QueryCurveUsageOptions.
ResultantCurveLocator
¶ Returns or sets the resultant curve locator
-------------------------------------
Getter Method
Signature
ResultantCurveLocator()
Returns: Return type: NXOpen.CAE.QueryCurveUsageOptionsResultantCurveLocatorType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResultantCurveLocator(resultantCurveLocator)
Parameters: resultantCurveLocator ( NXOpen.CAE.QueryCurveUsageOptionsResultantCurveLocatorType
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ResultantLocationTolerance¶
-
QueryCurveUsageOptions.
ResultantLocationTolerance
¶ Returns or sets the resultant location tolerance
-------------------------------------
Getter Method
Signature
ResultantLocationTolerance()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResultantLocationTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ReverseDirection¶
-
QueryCurveUsageOptions.
ReverseDirection
¶ Returns or sets the reverse direction
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)