ModelDisplayBuilderNodeDisplayModeType Enumeration¶
NXOpen.CAE.ModelDisplayBuilder.NodeDisplayModeType is an alias for NXOpen.CAE.ModelDisplayBuilderNodeDisplayModeType
-
class
NXOpen.CAE.
ModelDisplayBuilderNodeDisplayModeType
¶ Bases:
object
Indicates node display mode type.
Enum Members
Nodes attached to elements are shown when the elements are shown. Unattached nodes are always shown. “
“Explicit”, ” Nodes are explicitly shown and hidden via the Show/Hide commands. “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-