DurabilityRandomFatigueBuilderRandomFatigueMethodEnum Enumeration

NXOpen.CAE.DurabilityRandomFatigueBuilder.RandomFatigueMethodEnum is an alias for NXOpen.CAE.DurabilityRandomFatigueBuilderRandomFatigueMethodEnum

class NXOpen.CAE.DurabilityRandomFatigueBuilderRandomFatigueMethodEnum

Bases: object

the random method.

Enum Members

Enum Member Enum Member Description
NarrowBandMiles
NarrowBandMiles
WideBandDirlik
WideBandDirlik
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.