ResultComputationType Enumeration¶
NXOpen.CAE.Result.ComputationType is an alias for NXOpen.CAE.ResultComputationType
-
class
NXOpen.CAE.
ResultComputationType
¶ Bases:
object
types for different way of computing nodal result from element nodal result.
Enum Members
Enum Member Enum Member Description NotSet NoneAverage compute averageSum compute sum. (Applicable only for element-nodal vector result.)-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-