ModelDisplayBuilderStitchedEdgeWidth Enumeration

NXOpen.CAE.ModelDisplayBuilder.StitchedEdgeWidth is an alias for NXOpen.CAE.ModelDisplayBuilderStitchedEdgeWidth

class NXOpen.CAE.ModelDisplayBuilderStitchedEdgeWidth

Bases: object

specifies object width for display for geometry stitched edges

New in version NX8.5.0.

Enum Members

Enum Member Enum Member Description
Thin
Thin
Normal
Normal
Thick
Thick
One
Two
Three
Four
Five
Six
Seven
Eight
Nine
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.