GroupElemEdgeMethod Class¶
-
class
NXOpen.CAE.
GroupElemEdgeMethod
¶ Bases:
NXOpen.SelectionMethod
Represents the output from the Group Element Edge smart selector method
To obtain an instance of this class use CAE::SmartSelectionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetElementEdges | Returns the resultant element edges @return Resultant element edges |
GetSelectedObjects | Returns the objects selected by this NXOpen.SelectionMethod . |
Method Detail¶
Dispose¶
-
GroupElemEdgeMethod.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetElementEdges¶
-
GroupElemEdgeMethod.
GetElementEdges
¶ Returns the resultant element edges
Signature
GetElementEdges()
Returns: Resultant element edges Return type: list of NXOpen.CAE.FEElemEdge
New in version NX11.0.0.
License requirements: None.