CircularImprintBuilderAroundEdgeDiaType Enumeration

NXOpen.CAE.CircularImprintBuilder.AroundEdgeDiaType is an alias for NXOpen.CAE.CircularImprintBuilderAroundEdgeDiaType

class NXOpen.CAE.CircularImprintBuilderAroundEdgeDiaType

Bases: object

Around Edge Diameter Option

Enum Members

Enum Member Enum Member Description
Absolute
Absolute Diameter Value
Relative
Relative Value
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.