PostGraphBuilderGeometryValue Enumeration

NXOpen.CAE.PostGraphBuilder.GeometryValue is an alias for NXOpen.CAE.PostGraphBuilderGeometryValue

class NXOpen.CAE.PostGraphBuilderGeometryValue

Bases: object

This option is used to when the geometric entity selected has multiple result values.

This option applies to how we will resolve these multiple values into one

Enum Members

Enum Member Enum Member Description
Average
Minimum
Maximum
Sum
WeightedAverage
Integral
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.