MMCCreateBuilderTypes Enumeration

NXOpen.CAE.MMCCreateBuilder.Types is an alias for NXOpen.CAE.MMCCreateBuilderTypes

class NXOpen.CAE.MMCCreateBuilderTypes

Bases: object

Type of the Creation Methods for MMC

Enum Members

Enum Member Enum Member Description
AutoCreate
Auto Create
Manual
Manual Create
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.