CrossSectionParameters Class¶
-
class
NXOpen.CAE.
CrossSectionParameters
¶ Bases:
NXOpen.TaggedObject
This class is worked as a packet of information that can be used to change cross-section state.
<br/>Use
NXOpen.CAE.ResultManager
to create anNXOpen.CAE.CrossSectionParameters
To obtain an instance of this class use
NXOpen.Session.ResultManager()
.New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
GetAbsoluteValue | Ask whether all values are absolute values @return |
GetBeamElement | Ask beam element ID @return |
GetBeamEnd | Ask beam end @return |
GetComplexCriterion | If result is complex it returns which component is set(like real or imaginary) @return |
GetElementResult | Query Element Result value @return |
GetElementValueCriterion | Ask how element the result is defined. |
GetFilletRadius | Return the fillets flag @return |
GetFillets | Return the fillets flag @return |
GetGenericResultType | Ask Result type @return |
GetModelRangeParameters | Ask model range parameters @return |
GetPhaseAngle | Ask phase angle. |
GetResultComponent | Ask result component @return |
GetScale | Ask scale @return |
GetTensorComponentAbsoluteValue | Get the method used when calculating the absolute values for the derived components of NXOpen.CAE.ResultDataType.Tensor like NXOpen.CAE.ResultComponent.MaximumPrincipal @return |
GetUnit | Ask result unit @return |
MakeElementResult | Make Nodal result to Element Result. |
SetAbsoluteValue | Set all values to absolute values. |
SetBeamElement | Set beam element ID |
SetBeamEnd | Set beam end |
SetComplexCriterion | Set complex criteria |
SetElementValueCriterion | Set how element the result is defined |
SetFilletRadius | Turns on the fillets flag |
SetFillets | Turns on the fillets flag |
SetGenericResultType | Set Result type |
SetPhaseAngle | Sets the phase angle at which result will be evaluated. |
SetResultComponent | Set result component |
SetScale | Set scale. |
SetTensorComponentAbsoluteValue | Set the method used when calculating the absolute values for the derived components of NXOpen.CAE.ResultDataType.Tensor like NXOpen.CAE.ResultComponent.MaximumPrincipal |
SetUnit | Set result unit |
Method Detail¶
GetAbsoluteValue¶
-
CrossSectionParameters.
GetAbsoluteValue
¶ Ask whether all values are absolute values
Signature
GetAbsoluteValue()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetBeamElement¶
-
CrossSectionParameters.
GetBeamElement
¶ Ask beam element ID
Signature
GetBeamElement()
Returns: Return type: int New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetBeamEnd¶
-
CrossSectionParameters.
GetBeamEnd
¶ Ask beam end
Signature
GetBeamEnd()
Returns: Return type: NXOpen.CAE.ResultBeamEnd
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetComplexCriterion¶
-
CrossSectionParameters.
GetComplexCriterion
¶ If result is complex it returns which component is set(like real or imaginary)
Signature
GetComplexCriterion()
Returns: Return type: NXOpen.CAE.ResultComplex
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetElementResult¶
-
CrossSectionParameters.
GetElementResult
¶ Query Element Result value
Signature
GetElementResult()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetElementValueCriterion¶
-
CrossSectionParameters.
GetElementValueCriterion
¶ Ask how element the result is defined.
Signature
GetElementValueCriterion()
Returns: Return type: NXOpen.CAE.ResultElementValueCriterion
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetFilletRadius¶
-
CrossSectionParameters.
GetFilletRadius
¶ Return the fillets flag
Signature
GetFilletRadius()
Returns: Return type: float New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetFillets¶
-
CrossSectionParameters.
GetFillets
¶ Return the fillets flag
Signature
GetFillets()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetGenericResultType¶
-
CrossSectionParameters.
GetGenericResultType
¶ Ask Result type
Signature
GetGenericResultType()
Returns: Return type: NXOpen.CAE.BaseResultType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetModelRangeParameters¶
-
CrossSectionParameters.
GetModelRangeParameters
¶ Ask model range parameters
Signature
GetModelRangeParameters()
Returns: Return type: NXOpen.CAE.ResultParameters
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetPhaseAngle¶
-
CrossSectionParameters.
GetPhaseAngle
¶ Ask phase angle.
If complex result is set to Phaseangle type then user can specify an angle at which result will be evaluated
Signature
GetPhaseAngle()
Returns: Return type: float New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultComponent¶
-
CrossSectionParameters.
GetResultComponent
¶ Ask result component
Signature
GetResultComponent()
Returns: Return type: NXOpen.CAE.ResultComponent
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetScale¶
-
CrossSectionParameters.
GetScale
¶ Ask scale
Signature
GetScale()
Returns: Return type: float New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTensorComponentAbsoluteValue¶
-
CrossSectionParameters.
GetTensorComponentAbsoluteValue
¶ Get the method used when calculating the absolute values for the derived components of
NXOpen.CAE.ResultDataType.Tensor
likeNXOpen.CAE.ResultComponent.MaximumPrincipal
Signature
GetTensorComponentAbsoluteValue()
Returns: Return type: NXOpen.CAE.ResultTensorDerivedAbsolute
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetUnit¶
-
CrossSectionParameters.
GetUnit
¶ Ask result unit
Signature
GetUnit()
Returns: Return type: NXOpen.Unit
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
MakeElementResult¶
-
CrossSectionParameters.
MakeElementResult
¶ Make Nodal result to Element Result.
To define what value should be used to represent an element, use
NXOpen.CAE.CrossSectionParameters.SetElementValueCriterion()
Signature
MakeElementResult(elementResult)
Parameters: elementResult (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetAbsoluteValue¶
-
CrossSectionParameters.
SetAbsoluteValue
¶ Set all values to absolute values.
Warning: Once converted to absolute value it is not possible to revert to original values.
Signature
SetAbsoluteValue(absolute)
Parameters: absolute (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetBeamElement¶
-
CrossSectionParameters.
SetBeamElement
¶ Set beam element ID
Signature
SetBeamElement(beamEid)
Parameters: beamEid (int) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetBeamEnd¶
-
CrossSectionParameters.
SetBeamEnd
¶ Set beam end
Signature
SetBeamEnd(beamEnd)
Parameters: beamEnd ( NXOpen.CAE.ResultBeamEnd
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetComplexCriterion¶
-
CrossSectionParameters.
SetComplexCriterion
¶ Set complex criteria
Signature
SetComplexCriterion(complex)
Parameters: complex ( NXOpen.CAE.ResultComplex
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetElementValueCriterion¶
-
CrossSectionParameters.
SetElementValueCriterion
¶ Set how element the result is defined
Signature
SetElementValueCriterion(criteria)
Parameters: criteria ( NXOpen.CAE.ResultElementValueCriterion
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetFilletRadius¶
-
CrossSectionParameters.
SetFilletRadius
¶ Turns on the fillets flag
Signature
SetFilletRadius(filletRadius)
Parameters: filletRadius (float) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetFillets¶
-
CrossSectionParameters.
SetFillets
¶ Turns on the fillets flag
Signature
SetFillets(fillets)
Parameters: fillets (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetGenericResultType¶
-
CrossSectionParameters.
SetGenericResultType
¶ Set Result type
Signature
SetGenericResultType(type)
Parameters: type ( NXOpen.CAE.BaseResultType
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetPhaseAngle¶
-
CrossSectionParameters.
SetPhaseAngle
¶ Sets the phase angle at which result will be evaluated.
This is only value if complex result is set to the PhaseAngle type
Signature
SetPhaseAngle(angle)
Parameters: angle (float) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultComponent¶
-
CrossSectionParameters.
SetResultComponent
¶ Set result component
Signature
SetResultComponent(component)
Parameters: component ( NXOpen.CAE.ResultComponent
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetScale¶
-
CrossSectionParameters.
SetScale
¶ Set scale.
This will affect all subsequent result query.
Signature
SetScale(scale)
Parameters: scale (float) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetTensorComponentAbsoluteValue¶
-
CrossSectionParameters.
SetTensorComponentAbsoluteValue
¶ Set the method used when calculating the absolute values for the derived components of
NXOpen.CAE.ResultDataType.Tensor
likeNXOpen.CAE.ResultComponent.MaximumPrincipal
Signature
SetTensorComponentAbsoluteValue(absolute)
Parameters: absolute ( NXOpen.CAE.ResultTensorDerivedAbsolute
) –New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetUnit¶
-
CrossSectionParameters.
SetUnit
¶ Set result unit
Signature
SetUnit(unit)
Parameters: unit ( NXOpen.Unit
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)