ResultVariable Class¶
-
class
NXOpen.CAE.
ResultVariable
¶ Bases:
NXOpen.Fields.NameVariable
Controls Result Exp Object.
To obtain an instance of this class use CAE::ResultManager
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Abs | Returns or sets the Absolute value from result |
Addfillets | Returns or sets the Beam fillets |
BeamSect | Returns or sets the beam section |
Comp | Returns or sets the Component |
Complex | Returns or sets the Complex type |
Csys | Returns or sets the Co-ordinate System |
Derivebeamres | Returns or sets the Derive beam results |
Elementcriteria | Returns or sets the elemental result criteria |
Elemtypes | Returns or sets the Element types |
Expname | Returns the Result Field Expression Name |
Filletradscale | Returns or sets the Fillet radius scale factor |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer |
Loc | Returns or sets the Location |
Measure | Returns the measure of the variable |
Mids | Returns or sets the MIDs |
Name | Returns the name of the variable |
Nodalcombinetype | Returns or sets the Nodal Combination |
Numberofcomponent | Returns or sets the ply ID |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Phase | Returns or sets the Phase angle |
Pids | Returns or sets the PIDs |
Plyid | Returns or sets the ply ID |
Prototype | Returns the prototype of this object if it is an occurrence. |
Quan | Returns or sets the Quantity |
Selectedcsys | Returns or sets the Selected Co-ordinate System |
ShellSect | Returns or sets the shell section |
Tag | Returns the Tag for this object. |
Usertypename | Returns or sets the Result type username |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
Rename | Re-Name Result Variable |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
ResultVariableNodalCombination Enumeration | Element Nodal Combination Options |
Property Detail¶
Abs¶
-
ResultVariable.
Abs
¶ Returns or sets the Absolute value from result
-------------------------------------
Getter Method
Signature
Abs()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Abs(abs)
Parameters: abs (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Addfillets¶
-
ResultVariable.
Addfillets
¶ Returns or sets the Beam fillets
-------------------------------------
Getter Method
Signature
Addfillets()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Addfillets(addfillets)
Parameters: addfillets (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
BeamSect¶
-
ResultVariable.
BeamSect
¶ Returns or sets the beam section
-------------------------------------
Getter Method
Signature
BeamSect()
Returns: Return type: NXOpen.CAE.ResultSection
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
BeamSect(beamSect)
Parameters: beamSect ( NXOpen.CAE.ResultSection
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Comp¶
-
ResultVariable.
Comp
¶ Returns or sets the Component
-------------------------------------
Getter Method
Signature
Comp()
Returns: Return type: NXOpen.CAE.ResultComponent
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Comp(loc)
Parameters: loc ( NXOpen.CAE.ResultComponent
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Complex¶
-
ResultVariable.
Complex
¶ Returns or sets the Complex type
-------------------------------------
Getter Method
Signature
Complex()
Returns: Return type: NXOpen.CAE.ResultComplex
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Complex(complex)
Parameters: complex ( NXOpen.CAE.ResultComplex
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Csys¶
-
ResultVariable.
Csys
¶ Returns or sets the Co-ordinate System
-------------------------------------
Getter Method
Signature
Csys()
Returns: Return type: NXOpen.CAE.ResultCoordinateSystem
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Csys(csys)
Parameters: csys ( NXOpen.CAE.ResultCoordinateSystem
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Derivebeamres¶
-
ResultVariable.
Derivebeamres
¶ Returns or sets the Derive beam results
-------------------------------------
Getter Method
Signature
Derivebeamres()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Derivebeamres(derivebeamres)
Parameters: derivebeamres (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Elementcriteria¶
-
ResultVariable.
Elementcriteria
¶ Returns or sets the elemental result criteria
-------------------------------------
Getter Method
Signature
Elementcriteria()
Returns: Return type: NXOpen.CAE.ResultElementValueCriterion
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Elementcriteria(criteria)
Parameters: criteria ( NXOpen.CAE.ResultElementValueCriterion
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Elemtypes¶
-
ResultVariable.
Elemtypes
¶ Returns or sets the Element types
-------------------------------------
Getter Method
Signature
Elemtypes()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Elemtypes(elemtypes)
Parameters: elemtypes (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Expname¶
-
ResultVariable.
Expname
¶ Returns the Result Field Expression Name
-------------------------------------
Getter Method
Signature
Expname()
Returns: user will have to free name after use Return type: str New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Filletradscale¶
-
ResultVariable.
Filletradscale
¶ Returns or sets the Fillet radius scale factor
-------------------------------------
Getter Method
Signature
Filletradscale()
Returns: Return type: float New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Filletradscale(filletradscale)
Parameters: filletradscale (float) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
ResultVariable.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ResultVariable.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Layer¶
-
ResultVariable.
Layer
¶ Returns or sets the layer
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Loc¶
-
ResultVariable.
Loc
¶ Returns or sets the Location
-------------------------------------
Getter Method
Signature
Loc()
Returns: Return type: NXOpen.CAE.ResultLocation
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Loc(loc)
Parameters: loc ( NXOpen.CAE.ResultLocation
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Mids¶
-
ResultVariable.
Mids
¶ Returns or sets the MIDs
-------------------------------------
Getter Method
Signature
Mids()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Mids(mids)
Parameters: mids (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Nodalcombinetype¶
-
ResultVariable.
Nodalcombinetype
¶ Returns or sets the Nodal Combination
-------------------------------------
Getter Method
Signature
Nodalcombinetype()
Returns: Return type: NXOpen.CAE.ResultVariableNodalCombination
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Nodalcombinetype(computetype)
Parameters: computetype ( NXOpen.CAE.ResultVariableNodalCombination
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Numberofcomponent¶
-
ResultVariable.
Numberofcomponent
¶ Returns or sets the ply ID
-------------------------------------
Getter Method
Signature
Numberofcomponent()
Returns: Return type: int New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Numberofcomponent(numcomponent)
Parameters: numcomponent (int) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OwningComponent¶
-
ResultVariable.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ResultVariable.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Phase¶
-
ResultVariable.
Phase
¶ Returns or sets the Phase angle
-------------------------------------
Getter Method
Signature
Phase()
Returns: Return type: float New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Phase(phase)
Parameters: phase (float) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Pids¶
-
ResultVariable.
Pids
¶ Returns or sets the PIDs
-------------------------------------
Getter Method
Signature
Pids()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Pids(mids)
Parameters: mids (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Plyid¶
-
ResultVariable.
Plyid
¶ Returns or sets the ply ID
-------------------------------------
Getter Method
Signature
Plyid()
Returns: Return type: int New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Plyid(plyid)
Parameters: plyid (int) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Prototype¶
-
ResultVariable.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Quan¶
-
ResultVariable.
Quan
¶ Returns or sets the Quantity
-------------------------------------
Getter Method
Signature
Quan()
Returns: Return type: NXOpen.CAE.ResultQuantity
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Quan(quan)
Parameters: quan ( NXOpen.CAE.ResultQuantity
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Selectedcsys¶
-
ResultVariable.
Selectedcsys
¶ Returns or sets the Selected Co-ordinate System
-------------------------------------
Getter Method
Signature
Selectedcsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Selectedcsys(selectedcsys)
Parameters: selectedcsys ( NXOpen.CoordinateSystem
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ShellSect¶
-
ResultVariable.
ShellSect
¶ Returns or sets the shell section
-------------------------------------
Getter Method
Signature
ShellSect()
Returns: Return type: NXOpen.CAE.ResultSection
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ShellSect(sect)
Parameters: sect ( NXOpen.CAE.ResultSection
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Usertypename¶
-
ResultVariable.
Usertypename
¶ Returns or sets the Result type username
-------------------------------------
Getter Method
Signature
Usertypename()
Returns: user will have to free name after use Return type: str New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Usertypename(usertypename)
Parameters: usertypename (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
FindObject¶
-
ResultVariable.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
ResultVariable.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
Rename¶
-
ResultVariable.
Rename
¶ Re-Name Result Variable
Signature
Rename(expname)
Parameters: expname (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
ResultVariable.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.