PostGraphOrbitBuilder Class

class NXOpen.CAE.PostGraphOrbitBuilder

Bases: NXOpen.Builder

Represents a NXOpen.CAE.PostGraphOrbitBuilder

This is an abstract class and cannot be instantiated

New in version NX9.0.0.

Properties

Property Description
GraphTitle Returns or sets the graph title
Tag Returns the Tag for this object.
XresultComponent Returns or sets the component used as x axis for orbit plot
YresultComponent Returns or sets the component used as y axis for orbit plot

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
SetEntityIds Set entity ids for extracting result data
SetFreePoints Set free points for extracting data
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

GraphTitle

PostGraphOrbitBuilder.GraphTitle

Returns or sets the graph title

-------------------------------------

Getter Method

Signature GraphTitle()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

-------------------------------------

Setter Method

Signature GraphTitle(stringGraphTitle)

Parameters:stringGraphTitle (str) –

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

XresultComponent

PostGraphOrbitBuilder.XresultComponent

Returns or sets the component used as x axis for orbit plot

-------------------------------------

Getter Method

Signature XresultComponent()

Returns:
Return type:NXOpen.CAE.ResultComponent

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

-------------------------------------

Setter Method

Signature XresultComponent(xresult)

Parameters:xresult (NXOpen.CAE.ResultComponent) –

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

YresultComponent

PostGraphOrbitBuilder.YresultComponent

Returns or sets the component used as y axis for orbit plot

-------------------------------------

Getter Method

Signature YresultComponent()

Returns:
Return type:NXOpen.CAE.ResultComponent

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

-------------------------------------

Setter Method

Signature YresultComponent(yresult)

Parameters:yresult (NXOpen.CAE.ResultComponent) –

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

Method Detail

SetEntityIds

PostGraphOrbitBuilder.SetEntityIds

Set entity ids for extracting result data

Signature SetEntityIds(entityIds)

Parameters:entityIds (list of int) –

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

SetFreePoints

PostGraphOrbitBuilder.SetFreePoints

Set free points for extracting data

Signature SetFreePoints(freePoints)

Parameters:freePoints (list of NXOpen.Point3d) –

New in version NX9.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

Validate

PostGraphOrbitBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.