SimSimulationAxisymAbstractionType Enumeration¶
NXOpen.CAE.SimSimulation.AxisymAbstractionType is an alias for NXOpen.CAE.SimSimulationAxisymAbstractionType
-
class
NXOpen.CAE.
SimSimulationAxisymAbstractionType
¶ Bases:
object
Used to specify the axisymmetric abstraction type during solution creation.
Enum Members
Enum Member Enum Member Description NotSet No axisymmetric elements are allowedZxPlane ZX plane - Z axis axisymmetric elements are allowedXyPlane XY plane - Y axis axisymmetric elements are allowedXxyPlane XY plane - X axis axisymmetric elements are allowed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-