SimSolutionSolveOption Enumeration¶
NXOpen.CAE.SimSolution.SolveOption is an alias for NXOpen.CAE.SimSolutionSolveOption
-
class
NXOpen.CAE.
SimSolutionSolveOption
¶ Bases:
object
Solve Options
Enum Members
Enum Member Enum Member Description Solve write solver input file and launch solveWriteSolverInputFile write solver input file onlySolveInputFile launch solve with existing solver input fileWriteEditAndSolveInputFile write solver input file, allow edit and then launch solveEditSolverInputFile edit existing solver input fileSolveModelQualityResults solve model quality results-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-