SimRecipeCollection Class¶
-
class
NXOpen.CAE.
SimRecipeCollection
¶ Bases:
object
Provides methods for managing
NXOpen.CAE.SimRecipe
in a sim partTo obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateAutoBcRecipe | Creates a NXOpen.CAE.SimAutoBcRecipe @return Recipe created |
FindObject | Finds the NXOpen.CAE.SimRecipe with the given identifier as recorded in a journal. |
Method Detail¶
CreateAutoBcRecipe¶
-
SimRecipeCollection.
CreateAutoBcRecipe
¶ Creates a
NXOpen.CAE.SimAutoBcRecipe
Signature
CreateAutoBcRecipe(descriptorName, recipeName)
Parameters: - descriptorName (str) – Name of the Recipe descriptor
- recipeName (str) – Name of the Recipe
Returns: Recipe created
Return type: New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SimRecipeCollection.
FindObject
¶ Finds the
NXOpen.CAE.SimRecipe
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Recipe found Return type: NXOpen.CAE.SimRecipe
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)