PreTestExportUnvBuilderFileUnitsOption Enumeration

NXOpen.CAE.PreTestExportUnvBuilder.FileUnitsOption is an alias for NXOpen.CAE.PreTestExportUnvBuilderFileUnitsOption

class NXOpen.CAE.PreTestExportUnvBuilderFileUnitsOption

Bases: object

The unit type enum

Enum Members

Enum Member Enum Member Description
Si
SI: Meter (newton)
Bg
BG: Foot (pound f)
Mg
MG: Meter (kilogram f)
Ba
BA: Foot (poundal)
Mm
MM: mm (milli newton)
Cm
CM: cm (centi newton)
In
IN: Inch (pound f)
Gm
GM: mm (kilogram f)
Mn
MN: mm (newton)
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.