BaseIterationIterationValueType Enumeration¶
NXOpen.CAE.BaseIteration.IterationValueType is an alias for NXOpen.CAE.BaseIterationIterationValueType
-
class
NXOpen.CAE.
BaseIterationIterationValueType
¶ Bases:
object
The type of value that is stored in a iteration object
Enum Members
Enum Member Enum Member Description Unknown Value has an Unknown typeTime Value represents a TimeFrequency Value represents a FrequencyLoadFactor Value represents a LoadFactorEigenvalue Value represents a EigenvalueHarmonic Value represents a HarmonicRotationSpeed Value represents a RotationSpeed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-