AfuMathFastRMSOutput Class¶
-
class
NXOpen.CAE.
AfuMathFastRMSOutput
¶ Bases:
NXOpen.TransientObject
Represents the Fast RMS output information
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | The object destructor |
GetPsdfitFittedData | Returns fitted PSD data @return Frequency Value 2: Frequency Increment for Even Function |
GetPsdfitOriginalData | Returns PSD original data @return The Original PSD function y values |
GetRmsError | Returns the rms error @return The PSD fitting rms error |
SetPsdfitFittedData | |
SetPsdfitOriginalData | |
SetRmsError | Returns the rms error |
Method Detail¶
Dispose¶
-
AfuMathFastRMSOutput.
Dispose
¶ The object destructor
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetPsdfitFittedData¶
-
AfuMathFastRMSOutput.
GetPsdfitFittedData
¶ Returns fitted PSD data
Signature
GetPsdfitFittedData()
Returns: a tuple Return type: A tuple consisting of (psdfitFreqValue2, psdfitFittedX, psdfitFittedY, abcd, psdfitFreqValue1). psdfitFreqValue2 is a float. Frequency Value 2: Frequency Increment for Even Function psdfitFittedX is a list of float. the x values for the fitted PSD psdfitFittedY is a list of float. the y values for the fitted PSD abcd is a list of float. psdfitFreqValue1 is a float. Frequency Value 1: Minimum Freq for Even Function New in version NX11.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetPsdfitOriginalData¶
-
AfuMathFastRMSOutput.
GetPsdfitOriginalData
¶ Returns PSD original data
Signature
GetPsdfitOriginalData()
Returns: a tuple Return type: A tuple consisting of (psdfitOriginalY, psdfitOriginalX). psdfitOriginalY is a list of float. The Original PSD function y values psdfitOriginalX is a list of float. The Original PSD function x values New in version NX11.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetRmsError¶
-
AfuMathFastRMSOutput.
GetRmsError
¶ Returns the rms error
Signature
GetRmsError()
Returns: The PSD fitting rms error Return type: float New in version NX11.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
SetPsdfitFittedData¶
-
AfuMathFastRMSOutput.
SetPsdfitFittedData
¶ Signature
SetPsdfitFittedData(psdfitFittedX, psdfitFittedY, abcd, psdfitFreqValue1, psdfitFreqValue2)
Parameters: - psdfitFittedX (list of float) – The Fitted PSD X values
- psdfitFittedY (list of float) – The Fitted PSD Y values
- abcd (list of float) –
- psdfitFreqValue1 (float) –
- psdfitFreqValue2 (float) –
New in version NX11.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
SetPsdfitOriginalData¶
-
AfuMathFastRMSOutput.
SetPsdfitOriginalData
¶ Signature
SetPsdfitOriginalData(psdfitOriginalX, psdfitOriginalY)
Parameters: - psdfitOriginalX (list of float) – The Original PSD function x values
- psdfitOriginalY (list of float) – The Original PSD function y values
New in version NX11.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)