CorrelAlignmentBuilder Class¶
-
class
NXOpen.CAE.
CorrelAlignmentBuilder
¶ Bases:
NXOpen.CAE.CorrelBaseBuilder
This builder is used to control the alignment parameters of a
NXOpen.CAE.CorrelSolution
To create a new instance of this class, use
NXOpen.CAE.SimSolution.CreateAlignmentBuilder()
New in version NX6.0.1.
Properties¶
Property | Description |
---|---|
SaveXmlTransform | Returns or sets the save xml transform |
ScalingType | Returns or sets the scaling type |
ScalingValue | Returns or sets the scaling value |
Tag | Returns the Tag for this object. |
WrkPt1 | Returns or sets the working common origin point |
WrkPt2 | Returns or sets the working first axis origin point |
WrkPt3 | Returns or sets the working second axis point |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetReferencePt1 | Gets the reference common origin point @return |
GetReferencePt2 | Gets the reference first axis origin point @return |
GetReferencePt3 | Gets the reference second axis point @return |
SetReferencePt1 | Sets the reference common origin point |
SetReferencePt2 | Sets the reference first axis origin point |
SetReferencePt3 | Sets the reference second axis point |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CorrelAlignmentBuilderScalingChoice Enumeration | the way the scaling factor is computed |
Structs¶
CorrelAlignmentBuilderReferencePt_Struct Struct | Specifies the data for the selected reference points |
Property Detail¶
SaveXmlTransform¶
-
CorrelAlignmentBuilder.
SaveXmlTransform
¶ Returns or sets the save xml transform
-------------------------------------
Getter Method
Signature
SaveXmlTransform()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveXmlTransform(saveXmlTransform)
Parameters: saveXmlTransform (bool) – New in version NX9.0.0.
License requirements: nx_correl_base (“FE Correlation”)
ScalingType¶
-
CorrelAlignmentBuilder.
ScalingType
¶ Returns or sets the scaling type
-------------------------------------
Getter Method
Signature
ScalingType()
Returns: Return type: NXOpen.CAE.CorrelAlignmentBuilderScalingChoice
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingType(scalingType)
Parameters: scalingType ( NXOpen.CAE.CorrelAlignmentBuilderScalingChoice
) –New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
ScalingValue¶
-
CorrelAlignmentBuilder.
ScalingValue
¶ Returns or sets the scaling value
-------------------------------------
Getter Method
Signature
ScalingValue()
Returns: Return type: float New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingValue(scalingValue)
Parameters: scalingValue (float) – New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
WrkPt1¶
-
CorrelAlignmentBuilder.
WrkPt1
¶ Returns or sets the working common origin point
-------------------------------------
Getter Method
Signature
WrkPt1()
Returns: Return type: NXOpen.Point
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
WrkPt1(wrkPt1)
Parameters: wrkPt1 ( NXOpen.Point
) –New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
WrkPt2¶
-
CorrelAlignmentBuilder.
WrkPt2
¶ Returns or sets the working first axis origin point
-------------------------------------
Getter Method
Signature
WrkPt2()
Returns: Return type: NXOpen.Point
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
WrkPt2(wrkPt2)
Parameters: wrkPt2 ( NXOpen.Point
) –New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
WrkPt3¶
-
CorrelAlignmentBuilder.
WrkPt3
¶ Returns or sets the working second axis point
-------------------------------------
Getter Method
Signature
WrkPt3()
Returns: Return type: NXOpen.Point
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
WrkPt3(wrkPt3)
Parameters: wrkPt3 ( NXOpen.Point
) –New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
GetReferencePt1¶
-
CorrelAlignmentBuilder.
GetReferencePt1
¶ Gets the reference common origin point
Signature
GetReferencePt1()
Returns: Return type: NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct
New in version NX6.0.2.
License requirements: None.
GetReferencePt2¶
-
CorrelAlignmentBuilder.
GetReferencePt2
¶ Gets the reference first axis origin point
Signature
GetReferencePt2()
Returns: Return type: NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct
New in version NX6.0.2.
License requirements: None.
GetReferencePt3¶
-
CorrelAlignmentBuilder.
GetReferencePt3
¶ Gets the reference second axis point
Signature
GetReferencePt3()
Returns: Return type: NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct
New in version NX6.0.2.
License requirements: None.
SetReferencePt1¶
-
CorrelAlignmentBuilder.
SetReferencePt1
¶ Sets the reference common origin point
Signature
SetReferencePt1(referencePt1)
Parameters: referencePt1 ( NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct
) – Reference Point 1New in version NX6.0.2.
License requirements: nx_correl_base (“FE Correlation”)
SetReferencePt2¶
-
CorrelAlignmentBuilder.
SetReferencePt2
¶ Sets the reference first axis origin point
Signature
SetReferencePt2(referencePt2)
Parameters: referencePt2 ( NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct
) – Reference Point 2New in version NX6.0.2.
License requirements: nx_correl_base (“FE Correlation”)
SetReferencePt3¶
-
CorrelAlignmentBuilder.
SetReferencePt3
¶ Sets the reference second axis point
Signature
SetReferencePt3(referencePt3)
Parameters: referencePt3 ( NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct
) – Reference Point 3New in version NX6.0.2.
License requirements: nx_correl_base (“FE Correlation”)
Validate¶
-
CorrelAlignmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.