PostResultPreference Class¶
-
class
NXOpen.CAE.
PostResultPreference
¶ Bases:
object
Represents Post-Result Preferences
To obtain an instance of this class use CAE::CaePost::Preference
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ReadOneModeOrthogonalPair | Returns or sets the read one mode from Orthogonal-pair toggle |
Methods¶
Property Detail¶
ReadOneModeOrthogonalPair¶
-
PostResultPreference.
ReadOneModeOrthogonalPair
¶ Returns or sets the read one mode from Orthogonal-pair toggle
-------------------------------------
Getter Method
Signature
ReadOneModeOrthogonalPair()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ReadOneModeOrthogonalPair(readOneMode)
Parameters: readOneMode (bool) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)