LaminatePlyFilterBuilder Class

class NXOpen.CAE.LaminatePlyFilterBuilder

Bases: NXOpen.Builder

Represents a NXOpen.CAE.LaminatePlyFilterBuilder

There is no kf creator.

New in version NX8.0.0.

Properties

Property Description
SelectAllPlies Returns or sets the select all plies option
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
GetSelectedPlyNames Returns the selected plies
SetSelectedPlyNames Sets the selected plies
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

SelectAllPlies

LaminatePlyFilterBuilder.SelectAllPlies

Returns or sets the select all plies option

-------------------------------------

Getter Method

Signature SelectAllPlies()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: nx_lam_composites (“Laminate Composites”)

-------------------------------------

Setter Method

Signature SelectAllPlies(selectAllPlies)

Parameters:selectAllPlies (bool) –

New in version NX8.0.0.

License requirements: nx_lam_composites (“Laminate Composites”)

Method Detail

GetSelectedPlyNames

LaminatePlyFilterBuilder.GetSelectedPlyNames

Returns the selected plies

Signature GetSelectedPlyNames()

Returns:
Return type:list of str

New in version NX8.0.0.

License requirements: nx_lam_composites (“Laminate Composites”)

SetSelectedPlyNames

LaminatePlyFilterBuilder.SetSelectedPlyNames

Sets the selected plies

Signature SetSelectedPlyNames(selectedPlies)

Parameters:selectedPlies (list of str) –

New in version NX8.0.0.

License requirements: nx_lam_composites (“Laminate Composites”)

Validate

LaminatePlyFilterBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.