CreateJtBuilderComponent Enumeration¶
NXOpen.CAE.CreateJtBuilder.Component is an alias for NXOpen.CAE.CreateJtBuilderComponent
-
class
NXOpen.CAE.
CreateJtBuilderComponent
¶ Bases:
object
This option is used to set the component for export
Enum Members
Enum Member Enum Member Description Unknown Value has an Unknown typeCurrent Value represents component used to create result parameterPrimary Value represents all primary components-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-