ElementModifyOrderBuilderOperation Enumeration¶
NXOpen.CAE.ElementModifyOrderBuilder.Operation is an alias for NXOpen.CAE.ElementModifyOrderBuilderOperation
-
class
NXOpen.CAE.
ElementModifyOrderBuilderOperation
¶ Bases:
object
Represents the options for type of operation
Enum Members
Enum Member Enum Member Description Order changes the order of a mesh from linear to parabolic or vice versaMidnode changes the midnode option for a parabolic mesh to mixed, curved or linear-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-