FacetProximityBuilderDisplayOptions Enumeration

NXOpen.CAE.FacetProximityBuilder.DisplayOptions is an alias for NXOpen.CAE.FacetProximityBuilderDisplayOptions

class NXOpen.CAE.FacetProximityBuilderDisplayOptions

Bases: object

List option for facet proximity to UG CAD : NX7.

5 onwards

Enum Members

Enum Member Enum Member Description
LinearFacets
ParabolicFacets
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.