FemSynchronizeOptions Class¶
-
class
NXOpen.CAE.
FemSynchronizeOptions
¶ Bases:
NXOpen.TransientObject
Represents the synchronize options to be used when a FEM part is created These options will be used to synchronize the specified entities from the master CAD part file to the FEM part file
To create a new instance of this class, use
NXOpen.CAE.FemPart.NewFemSynchronizeOptions()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
SynchronizeArcsFlag | Returns or sets the synchronize arcs flag |
SynchronizeConicsFlag | Returns or sets the synchronize conics flag |
SynchronizeCoordinateSystemFlag | Returns or sets the synchronize coordinate system flag |
SynchronizeLinesFlag | Returns or sets the synchronize lines flag |
SynchronizePointsFlag | Returns or sets the synchronize points flag |
SynchronizeSketchCurvesFlag | Returns or sets the synchronize sketch curves flag |
SynchronizeSplinesFlag | Returns or sets the synchronize splines flag |
Methods¶
Method | Description |
---|---|
Dispose | Destroys the object |
SetAllSynchronizeFlags | Sets all the synchronize options to the given boolean value |
Property Detail¶
SynchronizeArcsFlag¶
-
FemSynchronizeOptions.
SynchronizeArcsFlag
¶ Returns or sets the synchronize arcs flag
-------------------------------------
Getter Method
Signature
SynchronizeArcsFlag()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SynchronizeArcsFlag(synchronizeOption)
Parameters: synchronizeOption (bool) – New in version NX4.0.0.
License requirements: None.
SynchronizeConicsFlag¶
-
FemSynchronizeOptions.
SynchronizeConicsFlag
¶ Returns or sets the synchronize conics flag
-------------------------------------
Getter Method
Signature
SynchronizeConicsFlag()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SynchronizeConicsFlag(synchronizeOption)
Parameters: synchronizeOption (bool) – New in version NX7.5.0.
License requirements: None.
SynchronizeCoordinateSystemFlag¶
-
FemSynchronizeOptions.
SynchronizeCoordinateSystemFlag
¶ Returns or sets the synchronize coordinate system flag
-------------------------------------
Getter Method
Signature
SynchronizeCoordinateSystemFlag()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SynchronizeCoordinateSystemFlag(synchronizeOption)
Parameters: synchronizeOption (bool) – New in version NX4.0.0.
License requirements: None.
SynchronizeLinesFlag¶
-
FemSynchronizeOptions.
SynchronizeLinesFlag
¶ Returns or sets the synchronize lines flag
-------------------------------------
Getter Method
Signature
SynchronizeLinesFlag()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SynchronizeLinesFlag(synchronizeOption)
Parameters: synchronizeOption (bool) – New in version NX4.0.0.
License requirements: None.
SynchronizePointsFlag¶
-
FemSynchronizeOptions.
SynchronizePointsFlag
¶ Returns or sets the synchronize points flag
-------------------------------------
Getter Method
Signature
SynchronizePointsFlag()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SynchronizePointsFlag(synchronizeOption)
Parameters: synchronizeOption (bool) – New in version NX4.0.0.
License requirements: None.
SynchronizeSketchCurvesFlag¶
-
FemSynchronizeOptions.
SynchronizeSketchCurvesFlag
¶ Returns or sets the synchronize sketch curves flag
-------------------------------------
Getter Method
Signature
SynchronizeSketchCurvesFlag()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SynchronizeSketchCurvesFlag(synchronizeOption)
Parameters: synchronizeOption (bool) – New in version NX4.0.0.
License requirements: None.
SynchronizeSplinesFlag¶
-
FemSynchronizeOptions.
SynchronizeSplinesFlag
¶ Returns or sets the synchronize splines flag
-------------------------------------
Getter Method
Signature
SynchronizeSplinesFlag()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SynchronizeSplinesFlag(synchronizeOption)
Parameters: synchronizeOption (bool) – New in version NX4.0.0.
License requirements: None.